AXIS#.HOME.MAXDIST

Description

AXIS#.HOME.MAXDIST sets the maximum distance the axis is allowed to move while homing. If the axis moves more that this distance without finding the home position the axis will decelerate to a stop and the W6023 warning will be generated. If AXIS#.HOME.MAXDIST is zero, then the maximum distance is not monitored and the axis will continue searching for the home position until commanded to stop.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Depends on AXIS#.UNIT.PROTARY :

Rotary: counts, rad, deg, custom units, 16-bit counts

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

Yes

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.MAXDIST

5008h

0ch

Unsigned32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6113

1

6113 (0x17e1)

AXIS1.HOME.MAXDIST

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.MAXDIST

6113

Signed32

Read/Write

Position

Variants Supported

All variants are supported.

Related Topics

Homing Terminology